Starwood, Turkey - Energy savings up to 22% with Eff-DRY smart automation app and retrofit
Starwood, Turkey - Energy savings up to 22% with Eff-DRY smart automation app and retrofit
Other manufacturing
STARWOOD ORMAN ÜRÜNLERİ SAN. AŞ
Bursa
The energy crisis in the world and therefore the increase in costs puts pressure on all companies. For this reason, the importance of energy efficiency is increasing day by day, especially energy-intensive areas like in the wood industry. Because of those reasons, Starwood wanted to enhance the overall energy efficiency by saving energy within their drying process in the MDF press line 1.
Starwood was searching for an energy efficiency solution partner to achieve these goals. That's why they reached out to Siemens because of the deep know-how on their processes and special process oriented energy efficiency solutions for all wood industries.
The dryer process is one of the most energy intensive processes in MDF plants. That's why the Siemens service experts used the Eff-DRY software to identify some savings potential. The process know-how and the software were developed by Siemens engineers and commissioned in the MDF plant with the use of a Sinamics GH180 Perfect Harmony drive (2250 kVA) and a new, state-of-the-art SIMATIC S7-300 PLC.
Technical
solution in detail:
SIMATIC S7-300 PLC and ET200 IO station
Eff-DRY automation algorithm (PLC) and Scada programming
Sinamics GH180 Perfect Harmony (2250 kVA) drive and commissioning
Measurement and verification for Energy
Performance Contracting
Instrumentation for velocity measurement of dusty hot air
The energy performance guarantee was given by Siemens and the before/after measurements and verification was done by certified Siemens Energy Efficiency Experts.
For the feasibility report, a detailed energy audit was performed by Siemens service experts according to ISO 50002. As a result of this report, 22% energy saving potential was identified by reducing the power consumtion from 1025 kW to 798.8 kW. This enables Starwood to save 990 tons of CO2 emissions per year. The payback time of the investment was calculated with 2.5 years.
Furthermore, by using the Eff-DRY software, the Siemens service experts were able to increase the production quality with regard to sensitive moisture control in the drying process.
Starwood,
engaged in the wood based panel board industry, is one of the biggest industrial
companies in Turkey with its growing production capacity and new investments
every year. The company has the highest production volume capacity in Turkey. It produces 2,000 m³ MDF per day on 2 lines and 3,000 m³ chipboard on 3 lines, which
is especially specialized in the production of thin MDF from 1.5 mm to 8 mm.
Starwood has a total production capacity of 220,000 m² in a 180,000 m² closed area
in the İnegöl plant and has a production capacity of 30,000 sheets / day with 8
short cycle press lines (dims 1830 mm and 2100 mm) together with a Georgian
plant.
Related Links
Please note that some of the links may be only available in Intranet.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.