Since Railway standards getting changes occasionally, SIPLUS extreme components go beyond these standards and are ready to meet more stringent future requirements.
Automation components (also fail-safe) that are certified to -25 °C and permit condensation.
The UPZ Group uses both standard and fail-safe SIPLUS extreme ET200SP controllers in its transportable barrier system. The barriers secure level crossings reliably even in the event of a power failure or cable breakage. When the transportable barrier system is used, the only personnel required is a temporary guard, thus enabling costs to be saved.
SIPLUS extreme components with Qualified Conformal Coating provide protection against mechanically active substances and an increased temperature range. This enables the controller to work reliably even under tough environmental conditions.
"And so it was clear from the very beginning that our main requirement was for a particularly rugged and resilient control system."
Andreas Ziemke - R&D Engineer
Customized
controller for customers needs. Mixed Failsafe and non Failsafe parts to get
the perfect solution
With SIPLUS extreme modules, the
customer is well equipped to meet future challenges in the railway industry
Siemens has been a partner in the
railway industry for years and provides solutions especially for harsh ambient
conditions
UPZ Sitech GmbH, the production company in the UPZ Group. This is where our especially developed products such as fixed barriers, signals, transportable temporary barriers, and air brake attachments are manufactured. The UPZ Group uses both standard and fail-safe SIPLUS extreme ET200SP controllers in its transportable barrier system. The barriers secure level crossings reliably even in the event of a power failure or cable breakage. When the transportable barrier system is used, the only personnel required is a temporary guard, thus enabling costs to be saved.
UPZ Group, Transportable barrier system with SIPLUS extreme
Rail industry, Germany
UPZ Group, Transportable barrier system with SIPLUS extreme
Rail industry, Germany
UPZ Group, Transportable barrier system with SIPLUS extreme
Completion: 2019
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Related Links
Please note that some of the links may be only available in Intranet.