Industrial Wireless LAN for Warehouse Logistics in Hot Strip Mill
Smooth Operation in harsh Industrial Environment
Machine Building
LogoTek GmbH
In the “hot storage” of the continuous casting plant, the material has a temperature of 700 °C.
Access Points with remote antennas had to be employed, which even under the harshest of conditions ensure a reliable operation of the local wireless network.
For the wireless network in the warehouse
buildings, IWLAN Access Points SCALANCE W774-1 were installed. A robust design and
minimal susceptibility to dirt, shock, and vibration are distinguishing
characteristics of the devices.
The distributed automation is implemented with
the peripheral system SIMATIC ET 200S.
“Even in a harsh industrial environment and under extreme climatic conditions, the systems operate with utmost reliability. The added value of the Siemens devices is clearly felt here.”
Managing director Matthias Knoke, LogoTek GmbH
The customer chose SCALANCE components from the IWLAN portfolio, because they provide an optimal combination of reliability and robustness.
The added value of the Siemens devices is clearly evident to the customer – they operate flawlessly even in a harsh industrial environment with extreme climatic conditions.
A Taiwanese steel group is general contractor for the construction of industrial plants. In Vietnam the company has erected a steel mill.