Stadtwerke Flensburg, Germany - Power Control Integration Services connect two worlds
Modernization plant with SIMATIC PCS 7 Station Gateway
Stadtwerke Flensburg, Germany - Power Control Integration Services connect two worlds
Power Utilities
Stadtwerke Flensburg GmbH
Flensburg Germany
Stadtwerke Flensburg was searching for a partner to modernize their plant. Their heavy-current side should be integrated into the SIMATIC PCS 7 world.
Furthermore, the customer has the following requirements:
One control system for both systems
High-availability system was
important
No external expertise for the heavy
current side
Use own SIMATIC PCS 7 expertise
Siemens Service experts provided the best possible solution based on the Power Control Integration Services.
SIMATIC PCS 7 Station Gateway was used forcoupling via IEC 61850 with the following details:
Integration of an existing SIPROTEC
medium-voltage switchgear with IEC61850-capable field devices in SIMATIC PCS 7
via Station Gateway
Solution from a single source using control system for joint monitoring and control of the processes and the
switchgear
Uniform control system for automation and switchgear (Switchgear is integrated into PCS 7 AS / OS)
Customer-specific adaptations for
displaying fast trip signals
High-availability connection
between the SIMATIC PCS 7 control system and the heavy-current side
Stadtwerke
Flensburg GmbH is the utility company of the city of Flensburg. Their business areas are electricity district heating, drinking water
industrial gas supply and telecommunications.