A suburban township in the upper Midwest United States buys their drinking water from a major municipal water district. The township’s water distribution system network has four connections to the larger municipality’s water transmission main. The municipality has many wholesale customers and has implemented contracts with each customer to limit the peak flows and the time of day in which they may occur. If a customer exceeds the limit, they are assessed significant surcharges.
These potential surcharges make it essential for wholesale customers to manage water demand prudently. As a result, many customers invest in solutions to minimize usage peaks and control what time of day they occur, including elevated water storage towers and control valves at each connection to the transmission main.
The major municipal water district owns and operates “metering pits” with electromagnetic flow meters (magmeters) immediately upstream of the control valves owned by each customer. However, as a rule, the signals from these meters are not made available to any customers on a real-time basis. Wholesale water customers are only provided with datalog summary reports from these meters on a routine schedule for billing purposes.
Without a method of measuring flow or receiving timely flow rate data from the water district, the suburban township had no means of knowing, in real time, the amount of water they were drawing from the transmission main. Therefore, they did not know if or when they were exceeding the contractual peak flowrate limits and incurring significant surcharges from the water district until they were billed.
The township needed to determine the flowrate at each of its four connections to the transmission main so that they could control how much was being drawn at each site. They also needed to know the total flow from the municipality’s transmission main so that they would not exceed their contractual peak demand.
The control valves were initially installed without flow
meters. The intention was to use valve position and
upstream/downstream (differential) pressure readings to
estimate the flow using the characteristic curve of the valve.
However, this proved to be too complicated and cumbersome
for the township‘s SCADA system to implement effectively.
The local Siemens representative worked with the township and
their engineer to find a solution to measure the flow rate and
totalize the volume of flow at each of the customer’s control valve
sites. The most significant challenge was the piping configuration,
as all of the valves were previously installed without proper
spacing for a flow meter.
The Siemens representative used a Siemens clamp-on ultrasonic
flow meter to demonstrate the technology to the customer and
prove that it would reliably meet their objectives. The valve with
the worst piping configuration was selected for the
demonstration, with the assumption that if the flow meter
would work for the worst site, it would work at the other three
sites as well. If the Siemens flow meter did not work for that site,
the township would need to consider alternate and more costly
flow measurement technologies.
Within minutes of arriving on site, the meter was installed and
providing reliable readings. The unit was allowed to log for a
period of three days. After that, the data was retrieved and
compared to the readings from a competitive magmeter in the
municipal water provider’s metering pit. The logger on the
Siemens clamp-on flow meter helped establish and solidify the
confidence of the owner and the engineer that the meter would
work for these applications.
The major benefits for the customer were cost savings, time savings and improved process reliability.
Cost savings: If the customer had been unable to use the Siemens clamp-on
ultrasonic flow meters, they would have had to excavate and
install a below-grade vault to house a magmeter and associated
isolation and bypass valves, along with conduit and wiring, at
each of the four sites. This would have required cutting the
water pipe and then going through a cumbersome disinfection
process, both of which would have required lengthy permitting
and costly testing.
Time savings: The customer had already made improvements to the
distribution system and installed four new control valves.
However, their construction contracts were closing and they
could not use their water tower until the new flow controls were
added, so time was a critical factor. The customer saved 3-6
months by using the Siemens clamp-on flow meters instead of
having to construct new vaults to house magmeters.
Improved process reliability: Now that the meters are in place, the customer can control how
much water they are taking from the water district at each of the
four locations and ensure that they do not exceed their
contractual peak. In addition, they can now properly manage the
fill and draw of their elevated storage tank to offset peak
demands, as well as during periods of low demand.
Township water authority uses clamp-on technology to avoid peak limit surcharges
Township water authority uses clamp-on technology to avoid peak limit surcharges
Release year: 2020
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Related Links
Please note that some of the links may be only available in Intranet.
Township water authority uses clamp-on technology to avoid peak limit surcharges