An energy storage facility in New York, USA, was
looking for a way to improve the efficiency of their power
generating turbines. During periods of peak demand the water is routed from the
upper to the lower reservoir making the turbines produce
power through gravitational forces only. When the demand
for water is low, the water is pumped back uphill using the
turbines and generators as pumps.
In order to improve the performance of the turbine it was
necessary to monitor the output efficiency by measuring
certain aspects of the application, such as flow and pressure.
These values are used to calculate the turbine performance
enabling plant operators to monitor the entire process and to
detect any trends and track changes over time.
One of the major issues at the energy facility was the
installation itself. Because of the way it was configured with
water flowing to the turbine during the day and water being
pumped back up to the reservoir at night, the solution had to
take this bi-directional flow into account. In addition, the pipe
diameter was so large and the pressures were so high that only one
flow technology was deemed fit for the job: ultrasonic clamp-on flow measurement.
A local Siemens area representative met with the energy storage facility and proposed the SITRANS FS230 clamp-on ultrasonic flow meter. Because of the sheer size, the space limitations and performance requirements of the application, the SITRANS FS230 clamp-on ultrasonic flow meter was the only suitable option. After extensive research, Siemens developed a
non-intrusive solution based on the FS230 clamp-on flow meter
that met the energy facility's requirements.
As a result of installing the FS230 ultrasonic clamp-on flow meter, the energy facility can now obtain accurate results and provide an exact picture of the turbine's performance.
Related Links
Please note that some of the links may be only available in Intranet.