Leakage currents and overheating of electronic equipment is caused by dust, pollution and corrosion. This can cause severe damage to converters, PLCs or other systems that work with scada-technology, which results in unplanned downtimes.
Furthermore, these kind of faults refer to unexpected costs, since they are usually detected after a long and expensive research.
Akzo Nobel wanted Siemens to provide a suitable preventive maintenance solution to avoid this kind of failures.
There are two different preventive cleaning methods available within the Siemens SIMAIN cleaning offering, according the plants conditions and degree contamination dry cleaning: This method is used if dust or similar contaminants are detected. These are removed with anti-static brushes and vacuum cleaners.
Wet cleaning (chemical liquid): It is used, when contaminations are not removable with the first method. Then the equipment is washed with chemical liquids. Furthermore, water purification with compressed air and dehumidification is done with a vacuum oven, before recommissioning.
The Siemens Service experts chose the wet cleaning method for the customers Micromaster 4 converters.
Detection of potential fault sources at an early stage
Reduction of corrective maintenance costs
Efficiency improvements with planned maintenances
Reduction of unexpected downtimes
We are a leading global supplier of performance coatings. Our products are essential for customers in a broad range of markets, including transportation, buildings, infrastructure, industrial and consumer goods. They are used by customers across the world to protect and enhance everything from ships, cars, aircraft, yachts and architectural components (structural steel, building products, flooring) to consumer goods (mobile devices, appliances, beverage cans, furniture) and industrial installations such as oil and gas facilities and wind turbines.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Akzo Nobel plant, Turkey - Reduced downtimes through SIMAIN cleaning