Skytanking has
several transfer pumps to pump Kerosine from storage tanks to the airplanes on
the tarmac. They
only have one main storage pump (flow ~16.000 liter/min) that is driven by a frequency converter which is obsolete as of October 2020. Since the customer has no more spare parts on stock and the availability of spare parts is restricted from now on the risk of an unplanned downtime increased. The
other three pumps are driven by smaller direct online (DOL) motors.
That's why Skytanking was searching for a reliable partner who can provide a suitable and fast retrofit solution. Furthermore, a Factory Acceptance Test (FAT) of the Profibus communication adaptions with the SIMATIC PCS 7 system should be done.
The planned downtime for the retrofit should not take longer than 24 hours and the SIMATIC PCS 7 system can only be in shutdown during the night which requires testing during night time.
Siemens service experts recommended to replace the old SINAMICS MASTERDRIVES with the successor out of the current SINAMICS familiy: The SINAMICS G120P cabinet which is an ideal solution for a pumping application. The ready-to-connect converter cabinet are available in the power ranges from 75 to 560 kW or from 315 to 630 kW and fit perfectly for the required performance and application.
The exisiting maintenance and spare parts contract for the SIMOVERT MASTERDRIVES was replaced by the same contract for the new SINAMICS G120P.
The project was deliverd as a turn-key project together with an electrical partner named Inarti.
"The trick is to leave as little as possible to chance ”
Pieter Reyniers, founder of our electrical partner
Inarti
Availability
of spare parts for many more years to come
Higher reliabiltiy due to state-of-the-art technology
SINAMICS converter family is ready for digitalization solutions
Hydrant Refuelling Systems (HRS) is a subsidiary of Skytanking. Skytanking provides a full range of aviation fuelling services including into-plane fuelling, aviation fuel storage and hydrant management, investment in aviation fuel facilities at airports and engineering. Its customers are airlines, airports and oil companies.
Skytanking kerosine pumps, Belgium - Fast and reliable retrofit of SIMOVERT MASTERDRIVES
Retrofit to Sinamics G120P gives wings to Skytanking (HRS)
Skytanking kerosine pumps, Belgium - Fast and reliable retrofit of SIMOVERT MASTERDRIVES
Retrofit to Sinamics G120P gives wings to Skytanking (HRS)
Completion: 2020
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Related Links
Please note that some of the links may be only available in Intranet.
Skytanking kerosine pumps, Belgium - Fast and reliable retrofit of SIMOVERT MASTERDRIVES