Starwood operates many motors in its plants. The eight existing motors, which were used in the particleboard production line, were old and consuming more energy, and operating inefficiently. As a result of a detailed energy audit, Siemens service experts offered a retrofit solution for these old motors.
Siemens service experts suggested replacing the inefficient motors with new, state-of-the-art, high-performance, low-voltage motors:
8 x SIMOTICS SD series 250kW IE4 motors
A detailed energy audit in accordance with ISO 50002 was carried out by Siemens service experts for the feasibility report. Reporting of the savings indicated in the feasibility report was done with post-implementation measurements. Measurement and verification were also established for the energy performance contract.
As a result of the feasibility report, an energy savings potential of 2.3 % with a payback period of 4.1 years was identified.
Further benefits:
Long-term availability of spare parts
Increased plant availability, productivity and relability
155.8 tons less CO2 emissions per year and 468 trees saved, thus reducing environmental impact
Electricity consumption reduced from 1565.5 kW to 1529.9 kW
Energy efficiency guaranteed by Siemens
Starwood, engaged in wood based
panel board industry, is one
of the biggest industrial companies in Turkey with its growing production
capacity and new investments every year. The company has the highest
production volume capacity in Turkey, produces 2,000 m³ MDF per day on 2
lines and 3,000 m³ chipboard 3 lines, which is especially specialized in the
production of thin MDF from 1.5 mm to 8 mm. Starwood has a total production
capacity of 220,000m² in 180.000m² closed area in İnegöl plant and has a
production capacity of 30,000 sheets / day with 8 short cycle press lines ( dims
1830 mm and 2100 mm) together with Georgian plant.
Related Links
Please note that some of the links may be only available in Intranet.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Starwood,Turkey – Energy efficiency increase enabled by IE4 SIMOTICS SD replacement
Starwood,Turkey – Energy efficiency increase enabled by IE4 SIMOTICS SD replacement
Starwood,Turkey – Energy efficiency increase enabled by IE4 SIMOTICS SD replacement