Tofas needed a service solution to reduce unplanned machine downtimes. Also they wanted to realize a just in time spare part storage and dynamic correction of maintenance plans.
Siemens provided a service solution through the Digitalization Implementation of Analyze MyCondition (AMC).
AMC is used for the condition based maintenance of machine tools. The customer can monitor the machine conditions online and use the data to plan maintenance activities. Related to condition based maintenance, the machine will inform the maintenance team by sending an e-mail before the occurring alarm.
Minimum loss of production due to condition based maintenance
Reduced maintenance time, maintenance costs and more effortless monitoring of machine conditions
Linking of signals, statuses and alarms on the CNC controller
Monitoring of CNC variables for limit value violations
Monitoring of measurement series for limit value violations
Fault message by the operator via the CNC controller HMI
<CompanyDescription>Founded in 1968, Tofaş is the only company in Turkey that manufactures both passenger cars and light commercial vehicles.
Tofaş is a Koç Holding and Fiat Chrysler Automobiles (FCA) partnership in which each controls an equal stake. With 24.3% of its capital publicly traded, Tofaş’s shares are included in both the Borsa İstanbul BIST 30 and the BIST 100 indexes as well as in exchange’s Corporate Governance Index and Sustainability indexes. Tofaş’s shares are also quoted on the Luxembourg Stock Exchange (LuxSE).</CompanyDescription>
Related Links
Please note that some of the links may be only available in Intranet.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Tofas plant, Turkey - Implementation of AMC minimizes production losses
Tofas plant, Turkey - Implementation of AMC minimizes production losses