The Triplast GmbH faces significant challenges in fire protection due to
the enormous fire load in its plastic sorting plants. The main cause
of this is lithium-ion batteries, which end up in plastic waste as
misthrows. These pose a dual risk: they ignite even with minor mechanical
damage and are extremely difficult to extinguish in case of fire due to
chemical reactions that intensify the blaze. Triplast's overriding objectives
are therefore to ensure maximum safety for people and machinery. This
includes the fastest possible detection of an ignition to effectively
prevent the spread of fire. This requires a fire protection system that
offers extreme reliability, sensitivity, and availability in fire
detection, and enables precise localization of the fire source.
Furthermore, a direct connection to the fire department is essential
to ensure a rapid response in an emergency.
Siemens was able to solve Triplast's complex fire protection
problem thanks to its innovative approaches tailored to the specific
challenges. Given the high fire load caused by lithium-ion batteries, a
solution was required that offered extreme reliability, sensitivity, and
availability in fire detection and enabled a rapid response.
The implemented solution is based on a superordinate FC2060 fire alarm
control panel, which forms the heart of the system. This is supplemented by two
sprinkler sub-control panels and a sprinkler pump control panel. Particularly
noteworthy is the use of over 300 neural fire detectors and nine thermal
imaging cameras. These state-of-the-art technologies are crucial for the early
and precise detection of hard-to-locate fire sources, such as lithium-ion
batteries, even before a fire can spread.
The comprehensive system is further strengthened by 56 flame detectors,
17 heat detectors, nine smoke detectors, and well over 100 manual call points
with integrated extinguishing release. The scale of the project is evident from
the multitude of alarming devices: 81 sirens, 87 strobe lights, 21 base
sounders, 97 alarm indicators, and 228 I/O modules for control and system
monitoring.
An efficient aspirating smoke detection system completes the monitoring.
In addition, the system is directly connected to the fire department, which is
automatically alerted if a fire alarm is not acknowledged within a predefined
time. This holistic solution not only ensures maximum safety but also enables a
quick and targeted response in the event of a fire.
"It clearly shows how important it is, for a plant of this size, to rely on an experienced partner who provides a modern solution for the optimal protection of our plant."
Fire protection for Triplast plastic sorting plants - Austria
DI Hubert Rammer, Project Manager, Bernegger GmbH
The comprehensive fire protection solution from Siemens ensures Triplast GmbH maximum safety for people and machinery. The fire alarm system has performed excellently to date and proves its exceptional sensitivity and reliability. The fact that the system triggers on average once a day underscores its ability for the earliest possible detection of potential fire sources, especially lithium-ion batteries. This is crucial to effectively prevent the spread of fires and thus avoid major damage and operational interruptions. Triplast benefits from significantly increased protection, which confirms the decision for Siemens as an experienced partner.
Triplast GmbH operates Europe's most modern and Austria's largest plastic sorting plant in Enns. As a joint venture of Altstoff Recycling Austria AG (ARA), Bernegger GmbH, and Der Grüne Punkt Holding, Triplast GmbH is a key player in plastic recycling. With an impressive sorting capacity of 100,000 tons of plastic per year, the company covers 50% of Austria's sorting capacity for lightweight packaging. Triplast GmbH thus makes a significant contribution to the European circular economy and sets new standards for plastic recycling in Austria. Its activities stand for plastic recycling at the highest level and a better future through innovative and efficient sorting processes.
Related Links
Please note that some of the links may be only available in Intranet.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.